GeomcopyBuilderCsysMirrorOptions Enumeration¶
NXOpen.Features.GeomcopyBuilder.CsysMirrorOptions is an alias for NXOpen.Features.GeomcopyBuilderCsysMirrorOptions
-
class
NXOpen.Features.
GeomcopyBuilderCsysMirrorOptions
¶ Bases:
object
CSYS mirror options
Enum Members
Enum Member Enum Member Description MirrorXAndY Mirror X and Y and derive ZMirrorYAndZ Mirror Y and Z and derive XMirrorZAndX Mirror X and Z and derive Y-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-