GeodesicProjectBuilderType Enumeration

NXOpen.Features.GeodesicProjectBuilder.Type is an alias for NXOpen.Features.GeodesicProjectBuilderType

class NXOpen.Features.GeodesicProjectBuilderType

Bases: object

Represents the type of objects projected to the support faces.

Enum Members

Enum Member Enum Member Description
Curve
Curves.
Point
Point.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.