GeodesicIntersectBuilderType Enumeration

NXOpen.Features.GeodesicIntersectBuilder.Type is an alias for NXOpen.Features.GeodesicIntersectBuilderType

class NXOpen.Features.GeodesicIntersectBuilderType

Bases: object

Represents the type of objects that intersect with the support faces.

Enum Members

Enum Member Enum Member Description
Datum
Datum.
Face
Face.
Curve
Curve.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.