FlatteningAndFormingBuilderDistortionMap Enumeration¶
NXOpen.Features.FlatteningAndFormingBuilder.DistortionMap is an alias for NXOpen.Features.FlatteningAndFormingBuilderDistortionMap
-
class
NXOpen.Features.
FlatteningAndFormingBuilderDistortionMap
¶ Bases:
object
Distortion Map options.
The options provides ability to display a distortion map on the source faces.
Enum Members
Enum Member Enum Member Description NotSet No distortion mapLength Distortion of lengthArea Distortion of areaAngle Shear distortion of U/V directions-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-