FaceBlendBuilderWidthMethod Enumeration

NXOpen.Features.FaceBlendBuilder.WidthMethod is an alias for NXOpen.Features.FaceBlendBuilderWidthMethod

class NXOpen.Features.FaceBlendBuilderWidthMethod

Bases: object

This enum represents the Face Blend width method, it is added in NX10 for two face blend

Enum Members

Enum Member Enum Member Description
NaturallyVarying
Naturally Varying
ForcedConstant
Forced Constant
TwoConstraintCurves
Two Constraint Curves
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.