FaceBlendBuilderDefiningType Enumeration

NXOpen.Features.FaceBlendBuilder.DefiningType is an alias for NXOpen.Features.FaceBlendBuilderDefiningType

class NXOpen.Features.FaceBlendBuilderDefiningType

Bases: object

This enum represents the Face Blend defining type, it is added in NX75 for new three face blend

Enum Members

Enum Member Enum Member Description
BlendTwoFace
this is for normal two face blend
BlendThreeFace
this is form new three face blend
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.