FaceBlendBuilderCrossSectionOption Enumeration

NXOpen.Features.FaceBlendBuilder.CrossSectionOption is an alias for NXOpen.Features.FaceBlendBuilderCrossSectionOption

class NXOpen.Features.FaceBlendBuilderCrossSectionOption

Bases: object

This enum represents the Cross section types

Enum Members

Enum Member Enum Member Description
Circular
Conic
this means tangent continuous asymmetric conic type
ConicSymmetric
this means tangent continuous symmetric conic type
CurvatureSymmetric
this means curvature continuous symmetric conic type
CurvatureAsymmetric
this means curvature continuous asymmetric conic type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.