ExtractFaceBuilderFeatureOptionType Enumeration

NXOpen.Features.ExtractFaceBuilder.FeatureOptionType is an alias for NXOpen.Features.ExtractFaceBuilderFeatureOptionType

class NXOpen.Features.ExtractFaceBuilderFeatureOptionType

Bases: object

enum for feature option type

Enum Members

Enum Member Enum Member Description
OneFeatureForAllBodies
An option to create one extracted or linked body feature for all selected bodies as body collector
SeparateFeatureForEachBody
An option to create a separate extracted or linked body feature per single body
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.