ExtractFaceBuilderFaceOptionType Enumeration

NXOpen.Features.ExtractFaceBuilder.FaceOptionType is an alias for NXOpen.Features.ExtractFaceBuilderFaceOptionType

class NXOpen.Features.ExtractFaceBuilderFaceOptionType

Bases: object

enum for face option type

Enum Members

Enum Member Enum Member Description
SingleFace
single face type
AdjacentFaces
adjacent face type
AllBodyFaces
all faces of body option
FaceChain
selection intent option
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.