EnlargeBuilderExtensionTypes Enumeration

NXOpen.Features.EnlargeBuilder.ExtensionTypes is an alias for NXOpen.Features.EnlargeBuilderExtensionTypes

class NXOpen.Features.EnlargeBuilderExtensionTypes

Bases: object

Extension types

Enum Members

Enum Member Enum Member Description
Linear
Linear extension
Natural
Natural extension
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.