EmbossRegionConvexityOption Enumeration¶
NXOpen.Features.EmbossRegion.ConvexityOption is an alias for NXOpen.Features.EmbossRegionConvexityOption
-
class
NXOpen.Features.
EmbossRegionConvexityOption
¶ Bases:
object
Describes whether the emboss geometry is above the target(“Pad”) or below the target(“Pocket”), or both(“Mixed”).
Enum Members
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-