EmbossProjection Class¶
-
class
NXOpen.Features.
EmbossProjection
¶ Bases:
NXOpen.TaggedObject
Represents a projection object.
Emboss projection object describes how to project section and to help build sidewall geometry.
Following are default values and options:
**Projection Option</b> :py:class:` Features.EmbossProjectionProjectionOption.Endcap < Features.EmbossProjectionProjectionOption>`
**Projection Face</b> User must set it when projection option is face.
**Projection Datum Plane</b> User must set it when projection option is plane.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Face | Returns or sets the projection face |
Option | Returns or sets the projection option |
Plane | Returns or sets the projection plane |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
EmbossProjectionProjectionOption Enumeration | Describes the geometry for projection |
Property Detail¶
Face¶
-
EmbossProjection.
Face
¶ Returns or sets the projection face
-------------------------------------
Getter Method
Signature
Face()
Returns: Faces for projection, if the projection option is :py:class:` Features.EmbossProjectionProjectionOption.Face < Features.EmbossProjectionProjectionOption>` Return type: NXOpen.ScCollector
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Face(projectionFace)
Parameters: projectionFace ( NXOpen.ScCollector
) – Faces for projection, if the projection option is :py:class:` Features.EmbossProjectionProjectionOption.Face < Features.EmbossProjectionProjectionOption>`New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Option¶
-
EmbossProjection.
Option
¶ Returns or sets the projection option
-------------------------------------
Getter Method
Signature
Option()
Returns: The projection option to decide where the profile projects. Return type: NXOpen.Features.EmbossProjectionProjectionOption
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
Option(option)
Parameters: option ( NXOpen.Features.EmbossProjectionProjectionOption
) – The projection option to decide where the profile projectsNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Plane¶
-
EmbossProjection.
Plane
¶ Returns or sets the projection plane
-------------------------------------
Getter Method
Signature
Plane()
Returns: Plane for projection, if the projection option is :py:class:` Features.EmbossProjectionProjectionOption.Plane < Features.EmbossProjectionProjectionOption>` Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane(projectionPlane)
Parameters: projectionPlane ( NXOpen.ISurface
) – Plane for projection, if the projection option is :py:class:` Features.EmbossProjectionProjectionOption.Plane < Features.EmbossProjectionProjectionOption>`New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)