EmbossLimit Class

class NXOpen.Features.EmbossLimit

Bases: NXOpen.TaggedObject

Represents emboss start and end objects, meaning, targets and end-cap definitions.

This class provides methods to set and get the various emboss limit sub components.

Following are default values and options:

**End-Cap Option</b> :py:class:` Features.EmbossLimitEndcapMethod.OffsetExact < Features.EmbossLimitEndcapMethod>`

**End-Cap Source Option</b> :py:class:` Features.EmbossLimitEndcapSourceOption.Target < Features.EmbossLimitEndcapSourceOption>`

**Emboss Target</b> (array) EmbossTarget object

**End-Cap Direction</b> Translate direction

**Distance</b> (translate or offset) 2.0/5.0[in/mm]

New in version NX4.0.0.

Properties

Property Description
Direction Returns or sets the direction for translation
Distance Returns the default distance for offset or translation
EndcapOption Returns or sets the endcap method to create the End-Cap
EndcapSource Returns or sets the endcap source option to decide where the End-Cap comes from
Tag Returns the Tag for this object.

Methods

Method Description
GetTargets The emboss targets @return Array of EmbossTarget object.
SetDistance The default distance expression formula string for offset or translation
SetTargets The emboss targets

Enumerations

EmbossLimitEndcapMethod Enumeration Describes the method that can be applied to the selected geometry to define the End-Cap.
EmbossLimitEndcapSourceOption Enumeration Describes the geometry that is used to create the End-Cap face/body.

Property Detail

Direction

EmbossLimit.Direction

Returns or sets the direction for translation

-------------------------------------

Getter Method

Signature Direction()

Returns:The direction for translation.
Return type:NXOpen.Direction

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Direction(direction)

Parameters:direction (NXOpen.Direction) – The direction for translation.

New in version NX4.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Distance

EmbossLimit.Distance

Returns the default distance for offset or translation

-------------------------------------

Getter Method

Signature Distance()

Returns:The default distance for offset or translation.
Return type:NXOpen.Expression

New in version NX4.0.0.

License requirements: None.

EndcapOption

EmbossLimit.EndcapOption

Returns or sets the endcap method to create the End-Cap

-------------------------------------

Getter Method

Signature EndcapOption()

Returns:The End-Cap method to create the End-Cap.
Return type:NXOpen.Features.EmbossLimitEndcapMethod

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EndcapOption(endcapOption)

Parameters:endcapOption (NXOpen.Features.EmbossLimitEndcapMethod) – The End-Cap method to create the End-Cap.

New in version NX4.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

EndcapSource

EmbossLimit.EndcapSource

Returns or sets the endcap source option to decide where the End-Cap comes from

-------------------------------------

Getter Method

Signature EndcapSource()

Returns:The End-Cap source option to decide where the End-Cap comes from.
Return type:NXOpen.Features.EmbossLimitEndcapSourceOption

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EndcapSource(endcapSourceOption)

Parameters:endcapSourceOption (NXOpen.Features.EmbossLimitEndcapSourceOption) – The End-Cap source option to decide where the End-Cap comes from.

New in version NX4.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

GetTargets

EmbossLimit.GetTargets

The emboss targets

Signature GetTargets()

Returns:Array of EmbossTarget object. In NX4, only one target is supported.
Return type:list of NXOpen.Features.EmbossTarget

New in version NX4.0.0.

License requirements: None.

SetDistance

EmbossLimit.SetDistance

The default distance expression formula string for offset or translation

Signature SetDistance(distance)

Parameters:distance (str) – The default distance expression formula string for offset or translation.

New in version NX4.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

SetTargets

EmbossLimit.SetTargets

The emboss targets

Signature SetTargets(targets)

Parameters:targets (list of NXOpen.Features.EmbossTarget) – Array of EmbossTarget object. In NX4, only one target is supported.

New in version NX4.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)