EmbossJoggleJoggleDirectionMethod Enumeration¶
NXOpen.Features.EmbossJoggle.JoggleDirectionMethod is an alias for NXOpen.Features.EmbossJoggleJoggleDirectionMethod
-
class
NXOpen.Features.
EmbossJoggleJoggleDirectionMethod
¶ Bases:
object
Describes the option that joggle direction along.
Enum Members
Enum Member Enum Member Description Sidewall Indicates joggle direction to along sidewall direction.Normal Indicates joggle direction to along normal of target.Specify Indicates joggle direction to along user specified direction-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-