EmbossBodyBuilder Class¶
-
class
NXOpen.Features.
EmbossBodyBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.EmbossBody
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateEmbossBodyBuilder()
Default values.
Property Value Clearance.Value 0 (millimeters part), 0 (inches part) ThickenOption True Thickness.Value 2 (millimeters part), 0.1 (inches part) New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CapFace | Returns or sets the cap face used to trim |
Clearance | Returns the emboss clearance |
KeepTargets | Returns or sets the copy targets flag |
KeepTools | Returns or sets the copy tools flag |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RegionObject | Returns the region object |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBody | Returns or sets the target body |
TargetMaterialSide | Returns or sets the target material side direction |
ThickenOption | Returns or sets the thicken option |
Thickness | Returns the emboss thickness |
ToolBody | Returns or sets the tool body |
ToolEmbossDirection | Returns or sets the tool emboss direction |
TrimOption | Returns or sets the trim option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CapFace¶
-
EmbossBodyBuilder.
CapFace
¶ Returns or sets the cap face used to trim
-------------------------------------
Getter Method
Signature
CapFace()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CapFace(capFace)
Parameters: capFace ( NXOpen.ScCollector
) –New in version NX8.5.0.
License requirements: None.
Clearance¶
-
EmbossBodyBuilder.
Clearance
¶ Returns the emboss clearance
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
KeepTargets¶
-
EmbossBodyBuilder.
KeepTargets
¶ Returns or sets the copy targets flag
-------------------------------------
Getter Method
Signature
KeepTargets()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepTargets(keepTargets)
Parameters: keepTargets (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
KeepTools¶
-
EmbossBodyBuilder.
KeepTools
¶ Returns or sets the copy tools flag
-------------------------------------
Getter Method
Signature
KeepTools()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepTools(keepTools)
Parameters: keepTools (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RegionObject¶
-
EmbossBodyBuilder.
RegionObject
¶ Returns the region object
-------------------------------------
Getter Method
Signature
RegionObject()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.5.0.
License requirements: None.
TargetBody¶
-
EmbossBodyBuilder.
TargetBody
¶ Returns or sets the target body
-------------------------------------
Getter Method
Signature
TargetBody()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetBody(targetBody)
Parameters: targetBody ( NXOpen.ScCollector
) –New in version NX8.5.0.
License requirements: None.
TargetMaterialSide¶
-
EmbossBodyBuilder.
TargetMaterialSide
¶ Returns or sets the target material side direction
-------------------------------------
Getter Method
Signature
TargetMaterialSide()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetMaterialSide(targetMaterialSide)
Parameters: targetMaterialSide (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ThickenOption¶
-
EmbossBodyBuilder.
ThickenOption
¶ Returns or sets the thicken option
-------------------------------------
Getter Method
Signature
ThickenOption()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThickenOption(thickenOption)
Parameters: thickenOption (bool) – New in version NX8.5.0.
License requirements: None.
Thickness¶
-
EmbossBodyBuilder.
Thickness
¶ Returns the emboss thickness
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ToolBody¶
-
EmbossBodyBuilder.
ToolBody
¶ Returns or sets the tool body
-------------------------------------
Getter Method
Signature
ToolBody()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolBody(toolBody)
Parameters: toolBody ( NXOpen.ScCollector
) –New in version NX8.5.0.
License requirements: None.
ToolEmbossDirection¶
-
EmbossBodyBuilder.
ToolEmbossDirection
¶ Returns or sets the tool emboss direction
-------------------------------------
Getter Method
Signature
ToolEmbossDirection()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolEmbossDirection(toolEmbossDirection)
Parameters: toolEmbossDirection (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TrimOption¶
-
EmbossBodyBuilder.
TrimOption
¶ Returns or sets the trim option
-------------------------------------
Getter Method
Signature
TrimOption()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimOption(trimOption)
Parameters: trimOption (bool) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
EmbossBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.