EditCrossSectionBuilder Class¶
-
class
NXOpen.Features.
EditCrossSectionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.EditCrossSection
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateEditCrossSectionBuilder()
Default values.
Property Value IncludeBlends 0 IncludeHoles 1 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Face | Returns the face collector. |
FaceChangeOverflowBehavior | Returns the face change overflow behavior. |
IncludeBlends | Returns or sets the include blends setting. |
IncludeHoles | Returns or sets the include holes setting. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Plane | Returns the select plane. |
SectionSketch | Returns or sets the sketch which holds the section curves |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ChangeSectionCurve | Change the section curves. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateSectionCurve | Create the section curves. |
DeleteSectionSketch | Remove the curve sketch |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
IncludeBlendFaces | Include or exclude the blends. |
IncludeHoleFaces | Include or exclude the holes. |
RecreateSectionCurve | Recreate the section curves. |
RemoveData | Remove the section data. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Face¶
-
EditCrossSectionBuilder.
Face
¶ Returns the face collector.
This holds all the input faces to intersect.
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FaceChangeOverflowBehavior¶
-
EditCrossSectionBuilder.
FaceChangeOverflowBehavior
¶ Returns the face change overflow behavior.
Please refer
NXOpen.GeometricUtilities.FaceChangeOverflowBehavior
for details.-------------------------------------
Getter Method
Signature
FaceChangeOverflowBehavior()
Returns: Return type: NXOpen.GeometricUtilities.FaceChangeOverflowBehavior
New in version NX8.0.0.
License requirements: None.
IncludeBlends¶
-
EditCrossSectionBuilder.
IncludeBlends
¶ Returns or sets the include blends setting.
True indicates a blend face participates in the section and is represented by a section curve.
-------------------------------------
Getter Method
Signature
IncludeBlends()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeBlends(includeBlends)
Parameters: includeBlends (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
IncludeHoles¶
-
EditCrossSectionBuilder.
IncludeHoles
¶ Returns or sets the include holes setting.
True indicates an interior boundary participates in the section and is represented in the section curve set.
-------------------------------------
Getter Method
Signature
IncludeHoles()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeHoles(includeHoles)
Parameters: includeHoles (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Plane¶
-
EditCrossSectionBuilder.
Plane
¶ Returns the select plane.
This is the plane to intersect.
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.SelectISurface
New in version NX8.0.0.
License requirements: None.
SectionSketch¶
-
EditCrossSectionBuilder.
SectionSketch
¶ Returns or sets the sketch which holds the section curves
-------------------------------------
Getter Method
Signature
SectionSketch()
Returns: Return type: NXOpen.Sketch
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionSketch(sectionSketch)
Parameters: sectionSketch ( NXOpen.Sketch
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
ChangeSectionCurve¶
-
EditCrossSectionBuilder.
ChangeSectionCurve
¶ Change the section curves.
Signature
ChangeSectionCurve()
New in version NX8.0.0.
License requirements: None.
CreateSectionCurve¶
-
EditCrossSectionBuilder.
CreateSectionCurve
¶ Create the section curves.
Signature
CreateSectionCurve()
New in version NX8.0.0.
License requirements: None.
DeleteSectionSketch¶
-
EditCrossSectionBuilder.
DeleteSectionSketch
¶ Remove the curve sketch
Signature
DeleteSectionSketch(sectionSketch)
Parameters: sectionSketch ( NXOpen.Sketch
) –New in version NX9.0.0.
License requirements: None.
IncludeBlendFaces¶
-
EditCrossSectionBuilder.
IncludeBlendFaces
¶ Include or exclude the blends.
Signature
IncludeBlendFaces()
New in version NX8.0.0.
License requirements: None.
IncludeHoleFaces¶
-
EditCrossSectionBuilder.
IncludeHoleFaces
¶ Include or exclude the holes.
Signature
IncludeHoleFaces()
New in version NX8.0.0.
License requirements: None.
RecreateSectionCurve¶
-
EditCrossSectionBuilder.
RecreateSectionCurve
¶ Recreate the section curves.
Signature
RecreateSectionCurve()
New in version NX8.0.0.
License requirements: None.
RemoveData¶
-
EditCrossSectionBuilder.
RemoveData
¶ Remove the section data.
Signature
RemoveData()
New in version NX8.5.0.
License requirements: None.
Validate¶
-
EditCrossSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.