EdgeSymmetryBuilderMovementMethods Enumeration

NXOpen.Features.EdgeSymmetryBuilder.MovementMethods is an alias for NXOpen.Features.EdgeSymmetryBuilderMovementMethods

class NXOpen.Features.EdgeSymmetryBuilderMovementMethods

Bases: object

Matching method options

Enum Members

Enum Member Enum Member Description
Normal
Does a normal match
Project
Does a match by projecting poles corresponding to target edge of the surface
WCS
Does a match by moving poles along a WCS principal axis direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.