DraftBuilderMethod Enumeration

NXOpen.Features.DraftBuilder.Method is an alias for NXOpen.Features.DraftBuilderMethod

class NXOpen.Features.DraftBuilderMethod

Bases: object

Describes the Draft type as true draft or isocline draft.

Enum Members

Enum Member Enum Member Description
Isocline
Indicates use of isocline algorithm to create draft. Default value.
TrueDraft
Indicates use of true draft algorithm to create draft.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.