DraftBodyBuilderTypes Enumeration

NXOpen.Features.DraftBodyBuilder.Types is an alias for NXOpen.Features.DraftBodyBuilderTypes

class NXOpen.Features.DraftBodyBuilderTypes

Bases: object

Describes the different Draft Body types

Enum Members

Enum Member Enum Member Description
Edges
From Edges
Faces
Faces to Draft
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.