DraftBodyBuilderMatchingType Enumeration¶
NXOpen.Features.DraftBodyBuilder.MatchingType is an alias for NXOpen.Features.DraftBodyBuilderMatchingType
-
class
NXOpen.Features.
DraftBodyBuilderMatchingType
¶ Bases:
object
Describes the different match types
Enum Members
Enum Member Enum Member Description NotSet No match type is specifiedToIsocline Match type IsoclineTangentToFace Match type Tangent to faceFromEdges Match type from edges-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-