DraftBodyBuilderMatchingScope Enumeration

NXOpen.Features.DraftBodyBuilder.MatchingScope is an alias for NXOpen.Features.DraftBodyBuilderMatchingScope

class NXOpen.Features.DraftBodyBuilderMatchingScope

Bases: object

Describes the different match scopes.

Enum Members

Enum Member Enum Member Description
All
All faces-to-draft are to be matched
AllButSelected
All faces-to-draft except the ones explicitly indicated are to be matched
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.