DivideCurveBuilderKnotPointOption Enumeration

NXOpen.Features.DivideCurveBuilder.KnotPointOption is an alias for NXOpen.Features.DivideCurveBuilderKnotPointOption

class NXOpen.Features.DivideCurveBuilderKnotPointOption

Bases: object

Represents the Divide Curve at Knot option types

Enum Members

Enum Member Enum Member Description
ByNumber
By Number
SelectPoint
Screen Position
AllKnotpoints
All Knotpoints
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.