DivideCurveBuilderInputArcLengthDirectionFlag Enumeration

NXOpen.Features.DivideCurveBuilder.InputArcLengthDirectionFlag is an alias for NXOpen.Features.DivideCurveBuilderInputArcLengthDirectionFlag

class NXOpen.Features.DivideCurveBuilderInputArcLengthDirectionFlag

Bases: object

Represents the Divide Curve Input Arc length direction flag

Enum Members

Enum Member Enum Member Description
Start
Input Arc length from start
End
Input Arc length from end
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.