DivideCurveBuilderEqualSegmentOption Enumeration

NXOpen.Features.DivideCurveBuilder.EqualSegmentOption is an alias for NXOpen.Features.DivideCurveBuilderEqualSegmentOption

class NXOpen.Features.DivideCurveBuilderEqualSegmentOption

Bases: object

Represents the Divide Curve equal segment method types

Enum Members

Enum Member Enum Member Description
EqualParameter
Equal Parameter
EqualArcLength
Equal Arc length
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.