DeleteFaceBuilderSetbackOptions Enumeration

NXOpen.Features.DeleteFaceBuilder.SetbackOptions is an alias for NXOpen.Features.DeleteFaceBuilderSetbackOptions

class NXOpen.Features.DeleteFaceBuilderSetbackOptions

Bases: object

Represents the set back options.

Enum Members

Enum Member Enum Member Description
SelectedBlend
Cap by setback along the selected blend.
NeighborBlend
Cap by setback along the neighbor of the selected blend.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.