DeleteFaceBuilderSelectTypes Enumeration

NXOpen.Features.DeleteFaceBuilder.SelectTypes is an alias for NXOpen.Features.DeleteFaceBuilderSelectTypes

class NXOpen.Features.DeleteFaceBuilderSelectTypes

Bases: object

Enumeration of select type, don’t use it until nx502

New in version NX5.0.2.

Enum Members

Enum Member Enum Member Description
Face
This stands for delete face type.
Hole
This stands for delete hole type.
Blend
This stands for delete blend type.
FaceEdgeBlend
This stands for delete notch blend type.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.