DeleteFaceBuilderFaceEdgeBlendPreferenceOptions Enumeration

NXOpen.Features.DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions is an alias for NXOpen.Features.DeleteFaceBuilderFaceEdgeBlendPreferenceOptions

class NXOpen.Features.DeleteFaceBuilderFaceEdgeBlendPreferenceOptions

Bases: object

Represents the face edge blend preference options.

Enum Members

Enum Member Enum Member Description
Notch
Delete as notch blend.
Cliff
Delete as cliff blend.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.