DeleteFaceBuilderCapOptionValues Enumeration

NXOpen.Features.DeleteFaceBuilder.CapOptionValues is an alias for NXOpen.Features.DeleteFaceBuilderCapOptionValues

class NXOpen.Features.DeleteFaceBuilderCapOptionValues

Bases: object

Represents the cap option values.

Enum Members

Enum Member Enum Member Description
FaceOrPlane
face or plane.
NewPlane
new plane.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.