DatumCsysBuilder Class¶
-
class
NXOpen.Features.
DatumCsysBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a datum csys builder
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateDatumCsysBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ComponentsCreation | Returns or sets the flag of the Datum Csys components creation |
Csys | Returns or sets the CSYS that defines a Datum CSYS |
DisplayScaleFactor | Returns or sets the scale factor of the input Datum Csys |
FixedSizeDatum | Returns or sets the fixed size flag of a created Datum Csys |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetWaveLinkInformation | Prints wave browser type information about link |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ComponentsCreation¶
-
DatumCsysBuilder.
ComponentsCreation
¶ Returns or sets the flag of the Datum Csys components creation
-------------------------------------
Getter Method
Signature
ComponentsCreation()
Returns: TRUE at creation and FALSE at edit Return type: bool New in version NX4.0.0.
Deprecated since version NX7.5.1: This property is now always TRUE and calls to this property can be safely removed.
License requirements: None.
-------------------------------------
Setter Method
Signature
ComponentsCreation(componentsCreation)
Parameters: componentsCreation (bool) – TRUE at creation and FALSE at edit New in version NX4.0.0.
Deprecated since version NX7.5.1: This property is now always TRUE and calls to this property can be safely removed.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Csys¶
-
DatumCsysBuilder.
Csys
¶ Returns or sets the CSYS that defines a Datum CSYS
-------------------------------------
Getter Method
Signature
Csys()
Returns: exisiting WCS Return type: NXOpen.CartesianCoordinateSystem
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys(csys)
Parameters: csys ( NXOpen.CartesianCoordinateSystem
) – exisiting WCS This parameter may not be None.New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
DisplayScaleFactor¶
-
DatumCsysBuilder.
DisplayScaleFactor
¶ Returns or sets the scale factor of the input Datum Csys
-------------------------------------
Getter Method
Signature
DisplayScaleFactor()
Returns: display scale factor Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayScaleFactor(displayScaleFactor)
Parameters: displayScaleFactor (float) – display scale factor New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
FixedSizeDatum¶
-
DatumCsysBuilder.
FixedSizeDatum
¶ Returns or sets the fixed size flag of a created Datum Csys
-------------------------------------
Getter Method
Signature
FixedSizeDatum()
Returns: always TRUE at both of creation and edit Return type: bool New in version NX4.0.0.
Deprecated since version NX7.5.1: This property is now always TRUE and calls to this property can be safely removed.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixedSizeDatum(fixedSizeDatum)
Parameters: fixedSizeDatum (bool) – always TRUE at both of creation and edit New in version NX4.0.0.
Deprecated since version NX7.5.1: This property is now always TRUE and calls to this property can be safely removed.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetWaveLinkInformation¶
-
DatumCsysBuilder.
GetWaveLinkInformation
¶ Prints wave browser type information about link
Signature
GetWaveLinkInformation()
Returns: a tuple Return type: A tuple consisting of (info, xformExists, xformOrigin, xformOrientation, xformScale). info is a str. queried wave information xformExists is a bool. true if there is a transform xformOrigin is a NXOpen.Point3d
. transformation origin xformOrientation is aNXOpen.Matrix3x3
. transformation matrix xformScale is a float. transformation scaleNew in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
Validate¶
-
DatumCsysBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.