DatumAxisBuilderUseArcLength Enumeration¶
NXOpen.Features.DatumAxisBuilder.UseArcLength is an alias for NXOpen.Features.DatumAxisBuilderUseArcLength
-
class
NXOpen.Features.
DatumAxisBuilderUseArcLength
¶ Bases:
object
Specifies points for which arclength is to be used.
Percentage of arclength is used for points for which arclength option is not selected. Specified for creation of datum axis using thru two points method.
Enum Members
Enum Member Enum Member Description NoPoint All points use percentage of arclengthFirstPoint Only first point uses arclengthSecondPoint Only second point uses arclengthAllPoints Both points use arclength-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-