DatumAxisBuilderFixedType Enumeration¶
NXOpen.Features.DatumAxisBuilder.FixedType is an alias for NXOpen.Features.DatumAxisBuilderFixedType
-
class
NXOpen.Features.
DatumAxisBuilderFixedType
¶ Bases:
object
Specifies the fixed type datum axis going thru only one specific axis or thru all axes.
Enum Members
Enum Member Enum Member Description All Fixed datum axis thru all AxisX Fixed datum axis thru X AxisY Fixed datum axis thru Y AxisZ Fixed datum axis thru Z Axis-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-