DatumAxisBuilderConstraintType Enumeration

NXOpen.Features.DatumAxisBuilder.ConstraintType is an alias for NXOpen.Features.DatumAxisBuilderConstraintType

class NXOpen.Features.DatumAxisBuilderConstraintType

Bases: object

Specifies different constraint types for selected geometries

Enum Members

Enum Member Enum Member Description
Undefined
Not defined
Coincident
Coincident constraint
Parallel
Parallel constraint
Perpendicular
Perpendicular constraint
Center
Center constraint
Tangent
Tangent constraint
Distance
Distance constraint
Angle
Angle constraint
Frenet
Frenet constraint
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.