DatumAxisBuilderAlternateSolution Enumeration¶
NXOpen.Features.DatumAxisBuilder.AlternateSolution is an alias for NXOpen.Features.DatumAxisBuilderAlternateSolution
-
class
NXOpen.Features.
DatumAxisBuilderAlternateSolution
¶ Bases:
object
Specifies the alternate solution for datum axis using point on curve method only
Enum Members
to a line, a datum axis, an edge of a solid, a planar face or a datum plane “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-