CustomFeatureSelectionFilter Class¶
-
class
NXOpen.Features.
CustomFeatureSelectionFilter
¶ Bases:
NXOpen.TransientObject
Represents a
Features.CustomFeatureSelectionFilter
classAn instance of this class can be obtained from
NXOpen.Features.CustomFeatureClassManager.CreateCustomFeatureSelectionFilter()
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the memory associated with this object. |
Filter | Custom Feature Selection Filter @return |
Method Detail¶
Dispose¶
-
CustomFeatureSelectionFilter.
Dispose
¶ Frees the memory associated with this object.
After invocation of this method, the object is no longer valid.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
Filter¶
-
CustomFeatureSelectionFilter.
Filter
¶ Custom Feature Selection Filter
Signature
Filter(objectToFilter)
Parameters: objectToFilter ( NXOpen.NXObject
) –Returns: Return type: int New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)