CustomFeaturePreUpdateEvent Class¶
-
class
NXOpen.Features.
CustomFeaturePreUpdateEvent
¶ Bases:
NXOpen.Features.CustomFeatureEvent
JA interface for the CustomFeaturePreUpdateEvent object
This calls cannot be created
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ErrorCode | Returns or sets the error occured during the event |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateConstructionFeatureData | Create construction feature data @return The object of ConstructionFeatureData |
GetConstructionFeatures | The custom feature get construction features @return Output array of NXOpen Features |
GetCustomFeature | Get the custom feature of the event @return The owning Custom Feature of feature that caused the event to fire |
GetNXObject | Get the Parasolid tag of Solid body @return |
GetOutputFeatures | The output features created in post update event @return Output array of NXOpen Features |
GetParasolidId | Get the Parasolid tag of Solid body @return |
SetConstructionFeatures | The custom feature construction features |
Method Detail¶
CreateConstructionFeatureData¶
-
CustomFeaturePreUpdateEvent.
CreateConstructionFeatureData
¶ Create construction feature data
Signature
CreateConstructionFeatureData(feature)
Parameters: feature ( NXOpen.Features.Feature
) – The feature for which the data object is to be createdReturns: The object of ConstructionFeatureData Return type: NXOpen.Features.ConstructionFeatureData
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetConstructionFeatures¶
-
CustomFeaturePreUpdateEvent.
SetConstructionFeatures
¶ The custom feature construction features
Signature
SetConstructionFeatures(constructionFeaturesTags)
Parameters: constructionFeaturesTags (list of NXOpen.Features.ConstructionFeatureData
) – Input array of NXOpen FeaturesNew in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)