CustomFeatureInformationEvent Class¶
-
class
NXOpen.Features.
CustomFeatureInformationEvent
¶ Bases:
NXOpen.Features.CustomFeatureEvent
JA interface for the CustomFeatureInformationEvent object
This calls cannot be created
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ErrorCode | Returns or sets the error occured during the event |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetConstructionFeatures | The custom feature get construction features @return Output array of NXOpen Features |
GetCustomFeature | Get the custom feature of the event @return The owning Custom Feature of feature that caused the event to fire |
GetNXObject | Get the Parasolid tag of Solid body @return |
GetOutputFeatures | The output features created in post update event @return Output array of NXOpen Features |
GetParasolidId | Get the Parasolid tag of Solid body @return |
SetInformation | The information about Custom Feature |