CopyPasteBuilderParentSelectOption Enumeration

NXOpen.Features.CopyPasteBuilder.ParentSelectOption is an alias for NXOpen.Features.CopyPasteBuilderParentSelectOption

class NXOpen.Features.CopyPasteBuilderParentSelectOption

Bases: object

Types of parent select option; Specifying smart object or selecting input for original parent

Enum Members

copied feature may be selected from the creation methods that were available on the original feature. “
“InputForOriginalParent”, ” Specifying smart object using the same creation method that was used in the original feature. “
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.