CopyPasteBuilderExpressionTransferOption Enumeration

NXOpen.Features.CopyPasteBuilder.ExpressionTransferOption is an alias for NXOpen.Features.CopyPasteBuilderExpressionTransferOption

class NXOpen.Features.CopyPasteBuilderExpressionTransferOption

Bases: object

Types of expression transfer mode

Enum Members

Enum Member Enum Member Description
CreateNew
New
LinkToOriginal
Link to Original
OriginalInstance
Instance of Original
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.