CopyPasteBuilderBuilderVersion Enumeration

NXOpen.Features.CopyPasteBuilder.BuilderVersion is an alias for NXOpen.Features.CopyPasteBuilderBuilderVersion

class NXOpen.Features.CopyPasteBuilderBuilderVersion

Bases: object

Types of version number

Enum Members

Enum Member Enum Member Description
Original
Value of original version; It can be set before NX8.0.
ExposeOnflySo
Value of version which exposes smart object created on fly as part of the copy operation; It should be set since NX8.0.
ExposeBody
Value of version which exposes additional target body parent; It should be added since NX8.5.
ShowParentSelectOption
Value of version which introduces parent select option; It should be added since NX8.5.1.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.