ConeBuilderTypes Enumeration

NXOpen.Features.ConeBuilder.Types is an alias for NXOpen.Features.ConeBuilderTypes

class NXOpen.Features.ConeBuilderTypes

Bases: object

Represents the Cone type

Enum Members

Enum Member Enum Member Description
DiametersAndHeight
Represents type of cone created by providing Diameters and Height
DiametersAndHalfAngle
Represents type of cone created by providing Diameters and Half Angle
BaseDiameterHeightAndHalfAngle
Represents type of cone created by providing Base Diameter, Height and Half Angle
TopDiameterHeightAndHalfAngle
Represents type of cone created by providing Top Diameter, Height and Half Angle
TwoCoaxialArcs
Represents type of cone created by providing Two Coaxial Arcs
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.