CompositeCurveBuilderPartType Enumeration

NXOpen.Features.CompositeCurveBuilder.PartType is an alias for NXOpen.Features.CompositeCurveBuilderPartType

class NXOpen.Features.CompositeCurveBuilderPartType

Bases: object

Composite Curve part type.

Enum Members

Enum Member Enum Member Description
WorkPart
Work part
OtherPart
Other part in assembly
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.