CompositeCurveBuilderJoinMethod Enumeration

NXOpen.Features.CompositeCurveBuilder.JoinMethod is an alias for NXOpen.Features.CompositeCurveBuilderJoinMethod

class NXOpen.Features.CompositeCurveBuilderJoinMethod

Bases: object

the join method

Enum Members

Enum Member Enum Member Description
No
No
Cubic
Cubic
Genernal
General
Quintic
Quintic
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.