ColorFeatureGroupBuilderProcessType Enumeration

NXOpen.Features.ColorFeatureGroupBuilder.ProcessType is an alias for NXOpen.Features.ColorFeatureGroupBuilderProcessType

class NXOpen.Features.ColorFeatureGroupBuilderProcessType

Bases: object

set color for new features only or set color and apply to all members

Enum Members

Enum Member Enum Member Description
NewFeatures
set color for new features only
AllMembers
set color and apply to all members
FirstLevelMembers
set color and apply to first level members
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.