BridgeCurveBuilderSurfaceDirectionTypes Enumeration

NXOpen.Features.BridgeCurveBuilder.SurfaceDirectionTypes is an alias for NXOpen.Features.BridgeCurveBuilderSurfaceDirectionTypes

class NXOpen.Features.BridgeCurveBuilderSurfaceDirectionTypes

Bases: object

This enum represents the direction type for input surfaces

Enum Members

of the base surface at the selected point “
“IsoU”, ” bridge direction takes u-isoparametric direction
of the base surface at the selected point “
“IsoV”, ” bridge direction takes v-isoparametric direction

of the base surface at the selected point “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.