BridgeCurveBuilderSelectedObject Enumeration

NXOpen.Features.BridgeCurveBuilder.SelectedObject is an alias for NXOpen.Features.BridgeCurveBuilderSelectedObject

class NXOpen.Features.BridgeCurveBuilderSelectedObject

Bases: object

This enum represents the current selected object for the bridge curve

Enum Members

Enum Member Enum Member Description
One
input object 1 selected
Two
input object 2 selected
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.