BridgeCurveBuilderExEndObjectTypes Enumeration

NXOpen.Features.BridgeCurveBuilderEx.EndObjectTypes is an alias for NXOpen.Features.BridgeCurveBuilderExEndObjectTypes

class NXOpen.Features.BridgeCurveBuilderExEndObjectTypes

Bases: object

End object type

Enum Members

Enum Member Enum Member Description
Section
Section
Object
A point or face
Datum
A datum plane or axis for symmetric constraint
Vector
A vector representing a plane for symmetric constraint
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.