BridgeCurveBuilderCurveDirectionTypes Enumeration

NXOpen.Features.BridgeCurveBuilder.CurveDirectionTypes is an alias for NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes

class NXOpen.Features.BridgeCurveBuilderCurveDirectionTypes

Bases: object

This enum represents the direction type for input curves

Enum Members

of the base curve at the selected point “
“Perpendicular”, ” bridge direction takes the direction that is

perpendicular to the tangent direction of the base curve at the selected point “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.