BridgeCurveBuilderConstraintTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilder.ConstraintTypes is an alias for NXOpen.Features.BridgeCurveBuilderConstraintTypes
-
class
NXOpen.Features.
BridgeCurveBuilderConstraintTypes
¶ Bases:
object
This enum represents the end continuity constraint types for the bridge curve
Enum Members
Enum Member Enum Member Description G0 G0 continuityG1 G1 continuityG2 G2 continuityG3 G3 continuity-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-