AssociativeLineBuilderEndReference Enumeration

NXOpen.Features.AssociativeLineBuilder.EndReference is an alias for NXOpen.Features.AssociativeLineBuilderEndReference

class NXOpen.Features.AssociativeLineBuilderEndReference

Bases: object

Represents references for end point

Enum Members

Enum Member Enum Member Description
Wcs
WCS
Absolute
Absolute
CordinatesSystem
CSYS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.