AssociativeArcBuilderStartOption Enumeration

NXOpen.Features.AssociativeArcBuilder.StartOption is an alias for NXOpen.Features.AssociativeArcBuilderStartOption

class NXOpen.Features.AssociativeArcBuilderStartOption

Bases: object

Represents start point options type

Enum Members

Enum Member Enum Member Description
Inferred
Inferred
Point
Point
Tangent
Tangent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.